Reply
Visitor
Posts: 3
Registered: ‎09-11-2015

Avnet Spartan-6/OMAP Co-Processing Development Kit - Programming SOM by External JTAG

Hi,

I want to program a DSP processor in OMAP-L138 SOM-M1 module by external JTAG. I have a Blackhawk XDS560v2-USB System Trace Emulator.

When I’m trying to program DSP I get an information from Code Compose Studio that DSP is held in reset - see attachment.

Is on the Avnet Spartan-6/OMAP Co-Processing Development Kit board any jumper or switch, that i have to setup to connect with DSP? DSP is held in reset.

I can’t find this Information in Started Guide.

Thanks.

Regards,

Lukasz.

1.png
Visitor
Posts: 3
Registered: ‎09-11-2015

Re: Avnet Spartan-6/OMAP Co-Processing Development Kit - Programming SOM by External JTAG

Finally I've got it.

1. Setup the Boot Mode for DSP-only Development -> Boot Mode = EMU DEBUG. DIP Switch on S7:

                8 = ON

                7 = OFF

                6 = OFF

                5 = ON

                4 = 3 = 2 = 1 = OFF.

2. Before start programming click switch SW 8 - Software RESET, and then you can load the program and debug it.

That's all.

Lukasz.

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: Avnet Spartan-6/OMAP Co-Processing Development Kit - Programming SOM by External JTAG

Awesome, glad you got it working !