Reply
Leo
Regular Visitor
Posts: 2
Registered: ‎09-20-2011

Error while compiling reference design

Hi,

 

I received my board recently and wanted to get familiar with the tools and environment, so I went ahead with the H/W Co-Simulation Reference Deisgn. I did everything up to the point where you want the generate the bit file from System Gen. After awhile, the compilation stops with the following error:

 

Partition Implementation Status
-------------------------------

  No Partitions were found in this design.

-------------------------------

NGDBUILD Design Results Summary:
  Number of errors:     0
  Number of warnings:  66

Writing NGD file "eth_cosim_top.ngd" ...
Total REAL time to NGDBUILD completion:  10 sec
Total CPU time to NGDBUILD completion:   10 sec

Writing NGDBUILD log file "eth_cosim_top.bld"...

NGDBUILD done.



#----------------------------------------------#
# Starting program map
# map -w -detail -o eth_cosim_top_map.ncd -intstyle xflow -timing -pr b -ol high
eth_cosim_top.ngd eth_cosim_top.pcf
#----------------------------------------------#
Using target part "6slx45tfgg484-2".
vvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvv
INFOSmiley Frustratedecurity:54 - 'xc6slx45t' is a WebPack part.
INFOSmiley Frustratedecurity:60 - The XILINXD_LICENSE_FILE environment variable is set to
'c:\Xilinx.lic'.
INFOSmiley Frustratedecurity:62 - The LM_LICENSE_FILE environment variable is set to
'c:\Xilinx.lic'.
INFOSmiley Frustratedecurity:68 - Please run the Xilinx License Configuration Manager
       (xlcm or "Manage Xilinx Licenses")
       to assist in obtaining a license.
ERRORSmiley Frustratedecurity:9 - No 'ISE' nor 'WebPack' feature was available for part
'xc6slx45t'.
----------------------------------------------------------------------
No such feature exists.
Feature:       WebPack
License path:
c:\Xilinx.lic;c:/xilinx/12.4/ise_ds/ise\coregen\core_licenses\Xilinx.lic;c:/xili
nx/12.4/ise_ds/ise\coregen\core_licenses\XilinxFree.lic;C:/.Xilinx\Xilinx.lic;c:
\xilinx\12.4\ise_ds\ise\/data\*.lic;C:\Xilinx\12.4\ISE_DS\EDK/data/core_licenses
\Xilinx.lic;
FLEXnet Licensing error:-5,357.  System Error: 2 ""
For further information, refer to the FLEXnet Licensing documentation,
available at "www.acresso.com".No such feature exists.
Feature:       ISE
License path:
c:\Xilinx.lic;c:/xilinx/12.4/ise_ds/ise\coregen\core_licenses\Xilinx.lic;c:/xili
nx/12.4/ise_ds/ise\coregen\core_licenses\XilinxFree.lic;C:/.Xilinx\Xilinx.lic;c:
\xilinx\12.4\ise_ds\ise\/data\*.lic;C:\Xilinx\12.4\ISE_DS\EDK/data/core_licenses
\Xilinx.lic;
FLEXnet Licensing error:-5,357
For further information, refer to the FLEXnet Licensing documentation,
available at "www.acresso.com".
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
ERROR:Map:258 - A problem was encountered attempting to get the license for this
   architecture.

Design Summary
--------------
Number of errors   :   1
Number of warnings :   0
ERROR:Xflow - Program map returned error code 2. Aborting flow execution...

 

I've check the licence I have using the xlcm and everything seems correct. I'm no expert in this. What could be the cause of this error ?

 

Thanks,

LM

Regular Contributor
Posts: 46
Registered: ‎07-09-2009

Re: Error while compiling reference design

Hi Leo,

 

can you post the results of "Xinfo"?
I'll take a look at that and see if I can fiigure out your problem.

 

B/r,

Russ

Leo
Regular Visitor
Posts: 2
Registered: ‎09-20-2011

Re: Error while compiling reference design

Hi,

 

Results of xinfo is attached.

 

Many thanks,

Leo

Highlighted
Visitor
Posts: 2
Registered: ‎02-06-2012

Re: Error while compiling reference design

Finally, and with the help of Xilinx, my problem was fixed. I had to regenerate the license file and make sure the Webpack component was part of the PACKAGE line.

 

Just thought I should let people of this forum know in case they run into the same problems.

 

LM