Reply
Highlighted
Visitor
Posts: 5
Registered: ‎02-22-2013

LOG_printf() Support

I have been attempting to work with DSPLink and found the reference code uses calls to LOG_printf()/  I was unable to see any output from these calls, so I tried adding them to the OOB reference design.  I couldn't get them to work there either.  Is the LOG_printf() and related functionality available on this board? I have the LOG section enabled in the TCF, and opened the RTDX Printf Logs window open (CCSv4).  I also don't ever see any updates to the CPU Load graph.  Could there be something else I need to configure or enable to get this to work?  Standard printf() calls work fine through the debugger.