Reply
sr
Regular Visitor
Posts: 2
Registered: ‎09-10-2009

OMAP UPP fpga interface

We are using spartan6 FPGA +OMAP based board. We are planning to use UPP interface between OMAP and FPGA.   We planned to use channel A as a bidirectional bus.  OMAP initially transmit some data (around 100 cycles) to FPGA and  later it will start receive data streaming from FPGA.  

My Question is is it possible to configure single channel as both transmitter and Receiver.

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: OMAP UPP fpga interface

SR,

 

The uPP DSP/BIOS driver required the UPP interface to configured as transmitter OR receiver.

During run-time initialization, the following call determines the direction of both of the uPP interfaces

   GIO_Handle upph = GIO_create("/UPP", IOM_INOUT, &status, &upp_setup, NULL);

 

Since the direction of the uPP interface is determined at run time, it should be possible to change the direction of the uPP interface by closing (GIO_delete), then re-initializing (GIO_create) the uPP interfaces.

However, you will need to ensure that the FPGA changes the pin directions and does not start transmitting until the DSP has re-initialized the interface ndd initiated a receive call.

 

Regards,

 

Mario.

 

Here are some very useful wiki pages on the subject of UPP.

 

uPP Peripheral

   http://processors.wiki.ti.com/index.php/Introduction_to_uPP

uPP Driver

   http://processors.wiki.ti.com/index.php/Using_the_uPP_DSP/BIOS_Driver

 

 

Newbie
Posts: 1
Registered: ‎08-14-2014

Re: OMAP UPP fpga interface

How quickly can the UPP bus be changed between read and write?  I don't see a spec in the datasheet for changing the bus from read to write.  What is the fastest the UPP bus can be turned around?