Reply
Contributor
Posts: 11
Registered: ‎07-04-2011

s6omapsdk installation problems

Hi,

 

I am trying to install the sdk on ubuntu 10.04 and following the getting started guide given by ridgerun. The installation never gets completed and the following error occurs:

 

Checking dependencies for gst-dmai-plugins
      Compiling and installing gst-dmai-plugins...
js: "/opt/s6omapsdk/proprietary/dvsdk_2_00_00/OMAP-L138_arm_1_00_00_11/codec_engine_2_25_00_05/packages/ti/sdo/ce/Engine.xs", line 328: Error: server info file '/opt/s6omapsdk/proprietary/dvsdk_2_00_00/OMAP-L138_arm_1_00_00_11/cs1omapl138_1_00_00/packages/ti/sdo/server/cs//package/info/./bin/cs.x674.info.js' does not exist; specified serverExecutable='./bin/cs.x674', serverPackage='ti.sdo.server.cs'; verify that your server package has been properly built and released.
    "/opt/s6omapsdk/proprietary/dvsdk_2_00_00/OMAP-L138_arm_1_00_00_11/codec_engine_2_25_00_05/packages/ti/sdo/ce/Engine.xs", line 341
    "/opt/s6omapsdk/proprietary/gst-dmai-plugins/src/src/omapl138.cfg", line 29
    "./package/cfg/omapl138_xv5T.cfg", line 474
    "./package/cfg/omapl138_xv5T.cfg", line 429
gmake: *** [package/cfg/omapl138_xv5T.c] Error 1
Warning: directory "/opt/s6omapsdk/proprietary/dvsdk_2_00_00/OMAP-L138_arm_1_00_00_11/local_power_manager_1_23_01/packages" on package path does not exist
Warning: directory "/soc/packages" on package path does not exist
Warning: directory "/opt/s6omapsdk/proprietary/codecs" on package path does not exist
Warning: directory "/opt/s6omapsdk/CodecServer" on package path does not exist
js: "/opt/s6omapsdk/proprietary/xdctools_3_16_01/xdctools_3_16_01_27/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
make[6]: *** [omapl138/linker.cmd] Error 1
make[5]: *** [all-recursive] Error 1
make[4]: *** [all] Error 2
make[3]: *** [build] Error 2
Error building gst-dmai-plugins
make[2]: *** [dependency_build] Error 1
make[1]: *** [proprietary_src_build] Error 1
make: *** [fs_build] Error 2

 

What could be the problem and how to resolve it.

 

With regards

Pankaj

Avnet Employee (Star Contributor)
Posts: 128
Registered: ‎04-20-2009

Re: s6omapsdk installation problems

I think that normally we do not install into /opt because that directory is typically written only by root.   Just a guess, but that could be the problem.  On your system, the error seems to be due to a missing file.  Is the file missing or is the entire directory or other set of files missing?

Avnet Employee (Star Contributor)
Posts: 128
Registered: ‎04-20-2009

Re: s6omapsdk installation problems

Disregard that last comment about /opt.  It's been a while since I've messed with this SDK.

Avnet Employee (Star Contributor)
Posts: 128
Registered: ‎04-20-2009

Re: s6omapsdk installation problems

However, the only thing that normally is installed in /opt is the toolchain.  All of the other stuff installs into $HOME.

Regular Visitor
Posts: 1
Registered: ‎10-26-2011

Re: s6omapsdk installation problems

Hello All,

 

I am also trying to build DVSDK(s6omapsdk-beta-Linux-x86-Install.bin) on ubuntu 10.04 LTS. Me too facing similar build issues as Pankaj. I tried to build in different folders i.e /opt and /home/omapl138 but the errors are same.Please help me if any one had overcome this problem.

 

js: "/home/omapl138/proprietary/xdctools_3_16_01/xdctools_3_16_01_27/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
make[6]: *** [omapl138/linker.cmd] Error 1
make[5]: *** [all-recursive] Error 1
make[4]: *** [all] Error 2
make[3]: *** [build] Error 2
Error building gst-dmai-plugins
make[2]: *** [dependency_build] Error 1
make[1]: *** [proprietary_src_build] Error 1
make: *** [fs_build] Error 2

Thanks

regards,

Sriram

Regular Visitor
Posts: 9
Registered: ‎12-09-2011

Re: s6omapsdk installation problems

Hi,

  I am also having some installation problems similar to previous posts. I am using Ubuntu 10.4 VM image from QuoTrader. I am  running through the getting started guide for the AVENET OMAPL138 EVM. I have run make several times and got down to the following errors,

 

user@ubuntu:~/s6omapsdk$ make

eth0: error fetching interface information: Device not found

  Ridgerun Linux SDK

  Board configuration: AVNET s6omap Board : OMAP-L138 - Xilinx Spartan 6

 

eth0: error fetching interface information: Device not found

  Processing toolchain...

    Build complete

eth0: error fetching interface information: Device not found

  Processing kernel...

  Kernel: arch/arm/boot/Image is ready

  Kernel: arch/arm/boot/zImage is ready

    Build complete

eth0: error fetching interface information: Device not found

  Processing fs...

    Checking for host packages required by the SDK target applications...

    Host machine has all required packages.

    Entering host-apps...

    Entering apps...

      Checking dependencies for alsa-lib-1.0.21

      Compiling and installing alsa-lib-1.0.21...

      Checking dependencies for alsa-utils-1.0.21

        Checking dependencies for ncurses-5.6

...

      Compiling and installing psplash...

      Checking dependencies for readline-5.2

      Compiling and installing readline-5.2...

    Entering /home/user/s6omapsdk/toolchain...

      Build complete

    Entering arch...

      Checking dependencies for base

      Compiling and installing base...

    Entering mach...

      Checking dependencies for base

      Compiling and installing base...

    Entering proprietary_src...

      Checking dependencies for dvsdk_2_00_00

        Checking dependencies for xdctools_3_16_01

        Compiling and installing xdctools_3_16_01...

      Compiling and installing dvsdk_2_00_00...

       Building cmem...

       Building cs1omapl138_1_00_00...

       Building dsplink...

       Building dmai...

make[3]: *** [dmai] Error 2

Error building dvsdk_2_00_00

make[2]: *** [dependency_build] Error 1

make[1]: *** [proprietary_src_build] Error 1

make: *** [fs_build] Error 2

user@ubuntu:~/s6omapsdk$

 

 

The eth0: erorrs may be due to running this on a laptop with a wireles and a cable ethernet port but do not know if this is going to cause me a final build error.

 

The final make[n] errors are baffeling me. Please can anyone suggest what to do next?

 

Regards,

  Kingfisher.

 

Avnet Employee (Star Contributor)
Posts: 114
Registered: ‎06-09-2009

Re: s6omapsdk installation problems

Hi Guys,

 

I am experiencing similar problems with the default SDK installation.  Let me investigate this a bit further with RidgeRun and I will post back to this thread with my results.

 

Regards,

 

-Kevin

Regular Visitor
Posts: 9
Registered: ‎12-09-2011

Re: s6omapsdk installation problems

Hi All,

  Just come back to this project and still having build problems. Anyone found a solution yet?