Reply
Highlighted
Visitor
Posts: 1
Registered: ‎08-06-2013

FMC150 external clock usage

Greetings all,

 

I am using the Avnet RTL reference design for the ML605 FMC150 interface. I want to implement the external clock function on the FMC150 board. More specifically, I would like the ADC to capture one bit of data everytime the external clock port receives a rising edge; the frequnecy of the external clock will vary. Can the FMC150 board achieve this function? If so, is there a reference design I should refer to? Alternatively, how do I modify the RTL reference design to enable this function. Your help would be greatly appreciated.

 

Best regards,

Schrasing