Reply
Highlighted
Regular Visitor
Posts: 5
Registered: ‎07-31-2014

ML605 unable to read from AMC7823 on FMC150

Hi, I cannot manage to read any register information back from AMC7823 chip on FMC150 board (all '0's), but things works fine for CDCE72010 read and write. I just like to confirm that the MON_SDO pin is located at H37 on the FMC150 connector as there are quite a few revesion of FMC150 and some doen't even have MON_N_INT. Also, I would like to confirm if this pin eventually connected with virtex 6 FPGA at pin N25, which is based on the reference design. Thank you.