Reply
Newbie
Posts: 1
Registered: ‎12-25-2017

Engineering Entrance Exams

The National Testing Agency or NTA will conduct all the national level engineering entrance exams along with other exams. The union cabinet has already approved this autonomous body recently. Now most of the exams are conducted by CBSE, AICTE and other agencies. The formation of NTA will help to reduce the burden of these bodies. It will also help to standardize the level of examination all over India. There is also a chance to conduct the national level examinations twice a year.

Highlighted
Newbie
Posts: 1
Registered: ‎10-04-2018

Re: Engineering Entrance Exams

You can find More Education Details here:

Students aspiring for JEE Main entrance exam need to gear up now to crack the test. Undoubtedly, JEE Main is an important engineering entrance examination which remains a prestigious one in India to secure admission rankings for reputed engineering institutions which offer quality technical education to the students. It is a proven fact that those students willing to make careers in engineering always dream to pass the JEE Main entrance.

JEE Advanced is a national level entrance exam is managed by the IIT, Kanpur. Through this exam, candidates will get admission into IITs & ISM. The examination consists of two papers, Paper 1 and Paper 2, each of three hours duration. Admission criteria of JEE Advanced 2019 has been released officially. The exam will be organized for admission in various undergraduate courses leading to a UG, Integrated PG or UG-PG Dual Degree. Such courses will be offered in the field of Engineering, Architecture, Sciences and/or Pharmaceutics. In fact, JEE Advanced 2019 is a national level entrance exam, which is managed by the IIT, Kanpur.

The sooner students processed online GATE Entrance Exam application, they were given this opportunity to rectify the mistakes if any during their application submission. They were given option for minor rectification in stipulated time frame from the days 13-17 November 2018. Candidates could opt for a change of examination city option.

It was simplified by asking them to log into GOAPS during those days to go ahead with making required changes. Applicants were advised to make additional payment of Rs.400/- for this purpose without which changes couldn’t be processed. Some colleges need State Entrance Score for some courses controlled and managed by state government.

Find best education details of India.
Newbie
Posts: 1
Registered: ‎10-25-2018

Re: Engineering Entrance Exams

Thanks for sharing the exams details, you can also check it here NTA UGC NET December 2018 if you want to apply.

Newbie
Posts: 6
Registered: ‎12-04-2018

Re: Engineering Entrance Exams

Ministry of Human Resource and Development announced the news that JEE Mains exam will be conducted by NTA, twice a year. The JEE Main 2019 examination will be conducted in multiple sessions from 6th January 2019 to 20th January 2019. It will be conducted online as a Computer Based Exam. No candidates would be allowed to appear in the examination in pen – paper mode. The aspirants can appear in both the examinations thus, they will not loose a time period of 1 year which was earlier the case. Showing enthusiasm toward the test, 9.65 lakh candidates have applied for JEE Main 2019 @ https://jeemainadmitcard2019.in/