Reply
Highlighted
Visitor
Posts: 14
Registered: ‎02-26-2018

Objects not visible when view port shading on solid or textu

Hi,

This may not actually be a Blender issue but I'm at a loss.
Blender 2.49 worked very well for me.
I'm running Ubuntu - Natty on an Aspire 2000
After upgrading to 2.5 and now 2.6 I have this issue.
Everything works as far as I can tell but I cannot see any object when the View port shading is set to solid or textured. The ground plan is not visible either. If I change the viewport shading to wireframe or bounding box everything is visible.
I tried going back to 2.49 but it didn't work at all.
Is it possibly an opengl problem ?

Any help will be apprecited.

I didn't find the right solution from the Internet.

References:
https://www.blender.org/forum/viewtopic.php?t=23665
Animated video production service

Thank you.

 

 

 

Newbie
Posts: 2
Registered: ‎06-24-2018

for AOL customer support

If you are facing AOL related issues then contact  AOL customer service executives who are available 24x7 to serve you. Get in touch at any hour of the day!