Reply
Avnet Employee (Regular Contributor)
Avnet Employee (Regular Contributor)
Posts: 25
Registered: ‎10-02-2009

Looking for Industrial Wi-Fi Module - 802.11 a/b/g/n/ac

[ Edited ]

Hello FAE team,

I am looking for the following in a module, or even better yet, a compete “dongle”.

End product: accessory for military radio. Basically providing Wi-Fi interface to existing military radios with USB port

  • EDITED: ADDING NEED FOR USB INTERFACE
  • Form factor: rugged dongle preferred, will look at industrial module that customer can enclose themselves
  • Industrial temp (-40 to +85 deg C) (Hitting -40 deg C with these specs is what makes this a little tougher)
  • 802.11 a/b/g/n/ac (no other wireless needed), 1x1 only
  • Linux drivers
  • Soft AP needed (number of connections not specified)
  • Timeframe: NOW
  • Volume: 1k-2.5k

Our local team is also digging into this however I wanted to cast a wider net.

Thanks!

Scott

Avnet Employee
Posts: 14
Registered: ‎10-21-2014

Re: Looking for Industrial Wi-Fi Module - 802.11 a/b/g/n/ac

Hi Scott-

Have you reached out to Suma Madapur regarding this need? She was updating our wireless module spreadsheet recently. Not too many suppliers are offering the /ac module, but they include Laird and Taiyo Yuden, as well as Murata.

-Tim

Avnet Employee (Regular Contributor)
Avnet Employee (Regular Contributor)
Posts: 25
Registered: ‎10-02-2009

Re: Looking for Industrial Wi-Fi Module - 802.11 a/b/g/n/ac

Just sent directly to Suma too...

Thx

Scott